In VB.NET,you can use the getData and putData functions shown in the IArrayTransfer interface. However, those functions return Variant data types, and VB.NET does not support Variant data types.
In this example, getData returns an "object", which is actually an "object[]" (array of object). Each object in the array is a "float". A new array of floats is created and then each instance is cast within the array to a float.
| Dim DataAsObject As Object Dim DataAsObjectArray(NumPoints - 1) As Object Dim ResultData (NumPoints - 1) As Double DataAsObject = na.Measurements.Item(1) DataAsObjectArray = DataAsObject.getData(AgilentPNA835x.NADataStore.naMeasResult, AgilentPNA835x.NADataFormat.naDataFormat_LogMag) For i As Integer = 0 To NumPoints - 1 ResultData(i) = CType(DataAsObjectArray(i), Double) Next i |