The following demonstrates how to:
Set the Source 1 Pulse Mod to enable
Set the Source 2 Pulse Mod to disable. In effect, this sets Source 2 to 'CW' (or OFF)
Set the Pulse Mod drive to Pulse1
See the entire list of IF Path Configuration settings.
|
' Create / Get the PNA application Dim app Set app = CreateObject("AgilentPNA835x.Application") ' Preset the instrument app.Preset ' Get a channel interface on which to operate Dim chan Set chan = app.ActiveChannel ' Set the Source 1 Pulse Mod to enable chan.PathConfiguration.Element("Src1Out1PulseModEnable").Value = "Enable" ' Set the Source 2 Pulse Mod to disable chan.PathConfiguration.Element("Src2Out1PulseModEnable").Value = "Disable" ' Set the Pulse Mod drive to Pulse1 chan.PathConfiguration.Element("PulseModDrive").Value = "Pulse1" |