The following example performs a 2-port or 4-port Guided Cal using C#.
Note: Replace <remote host name> with the full computer name of your PNA.
Learn more about using .NET with the PNA
|
AgilentPNA835x.IApplication pna; AgilentPNA835x.ICalManager3 calMgr; AgilentPNA835x.IGuidedCalibration guidedCal; AgilentPNA835x.IChannel chan; int chanNum; AgilentPNA835x.ICalSet calset; void PerformGuidedCal() { Type pnaType = Type.GetTypeFromProgID("AgilentPNA835x.Application", "<remote host name>"); pna = (AgilentPNA835x.IApplication) Activator.CreateInstance(pnaType); calMgr = (AgilentPNA835x.ICalManager3)pna.GetCalManager(); guidedCal = (AgilentPNA835x.IGuidedCalibration)calMgr.GuidedCalibration; chan = pna.ActiveChannel; chanNum = chan.channelNumber; // Initialize guided cal to be performed on the active channel. // The boolean argument of True indicates to store the cal only // in the channel's calibration register. If instead you wish // to create a new calset that the new cal will get stored to, // comment out this next line and uncomment the three lines below it. guidedCal.Initialize(chanNum, true); calset = calMgr.CreateCalSet(chanNum); chan.SelectCalSet(calset.GetGUID(), true); guidedCal.Initialize(chanNum, false);
// To perform 2-port cal, Uncomment the following // Then comment the 4-port cal
// Do 2-port cal // TwoPortGuidedCal();
// Do 4-port cal FourPortGuidedCal(); }
void TwoPortGuidedCal() { // Select the connectors guidedCal.set_ConnectorType(1, "APC 3.5 female"); guidedCal.set_ConnectorType(2,"APC 3.5 male"); for (int i = 3; i <= pna.NumberOfPorts; i++) guidedCal.set_ConnectorType(i, "Not used"); MessageBox.Show("Connectors defined for Ports 1 and 2"); // Select the Cal Kit for each port being calibrated. guidedCal.set_CalKitType(1,"85052D"); guidedCal.set_CalKitType(2,"85052D"); // To use an ECal module instead, comment out the above two lines // and uncomment the following two lines. // Replace N4691-60004 with your own ECAL model followed by 'ECal'. // Your ECal module must already be connected to a PNA USB port. // guidedCal.CalKitType(1) = "N4691-60004 ECal" // guidedCal.CalKitType(2) = "N4691-60004 ECal" MessageBox.Show("Cal kits defined for Ports 1 and 2"); // Initiate the calibration and query the number of steps int numSteps = guidedCal.GenerateSteps(); // Measure the standards, compute and apply the cal MeasureAndComplete(numSteps); }
void FourPortGuidedCal() { //Select the connectors guidedCal.set_ConnectorType(1,"APC 3.5 female"); guidedCal.set_ConnectorType(2,"APC 3.5 female"); guidedCal.set_ConnectorType(3,"APC 3.5 female"); guidedCal.set_ConnectorType(4,"APC 3.5 female"); // If a PNA which has more than 4 ports for (int i = 5;i<=pna.NumberOfPorts;++i) guidedCal.set_ConnectorType(i,"Not used");
MessageBox.Show("Connectors defined for Ports 1 to 4"); // Select the Cal Kit for each port being calibrated. guidedCal.set_CalKitType(1,"85052D"); guidedCal.set_CalKitType(2,"85052D"); guidedCal.set_CalKitType(3,"85052D"); guidedCal.set_CalKitType(4, "85052D"); // To use an ECal module instead, comment out the above four lines // and uncomment the following four lines. // Replace N4691-60003 with your own ECAL model followed by 'ECal'. // Your ECal module must already be connected to a PNA USB port. //guidedCal.CalKitType(1) = "N4431-60003 ECal"; //guidedCal.CalKitType(2) = "N4431-60003 ECal"; //guidedCal.CalKitType(3) = "N4431-60003 ECal"; //guidedCal.CalKitType(4) = "N4431-60003 ECal"; MessageBox.Show("Cal kits defined for Ports 1 to 4"); // Initiate the calibration guidedCal.GenerateSteps(); // If your selected cal kit is not a 4-port ECal module which can // mate to all 4 ports at once, then you may want to choose which // thru connections to measure for the cal. You must measure at // least 3 different thru paths for a 4-port cal (for greatest // accuracy you can choose to measure a thru connection for all 6 // pairings of the 4 ports). If you omit this command, the default // is to measure from port 1 to port 2, port 1 to port 3, and // port 1 to port 4. For this example we select to measure // from port 1 to port 2, port 2 to port 3, and port 2 to port 4. long[] portList = new long[6]{1,2,2,3,2,4}; guidedCal.ThruPortList = portList; // Re-generate the connection steps to account for the thru changes int numSteps = guidedCal.GenerateSteps(); // Measure the standards, compute and apply the cal MeasureAndComplete(numSteps); }
void MeasureAndComplete(int numSteps) { MessageBox.Show("Number of steps is " + numSteps.ToString());
// Measure the standards // The following series of commands shows that standards // can be measured in any order. These steps acquire // measurement of standards in reverse order. // It is easiest to iterate through standards using // a For-Next Loop. for (int i = numSteps; i >= 1; --i) { string strPrompt = guidedCal.GetStepDescription(i); MessageBox.Show(strPrompt); guidedCal.AcquireStep(i); }
// Conclude the calibration guidedCal.GenerateErrorTerms(); MessageBox.Show("Cal is done!"); } |