The Code Translator (CXL) Application allows you to control the PNA using your 8753, 872x, or 8510 (Legacy) GPIB test programs. The CXL Application runs on the PNA and processes each legacy command, real time, by first recognizing it as a valid legacy commands, and then executing the equivalent PNA command if one exists. The CXL Application will also help translate your Legacy programs into PNA SCPI and COM commands.
The CXL Application works with HP-VEE, Visual Basic, and RMB programs. The CXL Application must be used with PNA revision firmware A.04.00 or later.
New When cXL is installed on the PNA, a quick menu link is provided to launch the cXL. To use the link:
Press System, then [Configure], then [Code Emulation]
Installing the CXL Application
Download the CXL application from http://na.support.keysight.com/pna/cxl.html. To install the CXL application, double click on the InstallShield package icon.
The CXL application has its own help file that includes a command cross-reference for 8510/8753/872x models to PNA commands.