Setup the Display using SCPI


This Visual Basic program:

To run this program, you need:

See Other SCPI Example Programs

GPIB.Write "SYSTem:PRESet"

'Select the measurement

GPIB.Write "CALCulate:PARameter:SELect 'CH1_S11_1'"


'Set the Data Format to Log Mag

GPIB.Write ":CALCulate1:FORMat MLOG"


'Turn ON the Trace, Title, and Frequency Annotation

GPIB.Write "Display:WINDow1:TRACe1:STATe ON"
GPIB.Write "DISPlay:WINDow1:TITLe:STATe ON"
GPIB.Write "DISPlay:ANNotation:FREQuency ON"


'Autoscale the Trace

GPIB.Write "Display:WINDow1:TRACe1:Y:Scale:AUTO"


'Query back the Per Division, Reference Level, and Reference Position

GPIB.Write "DISPlay:WINDow1:TRACe1:Y:SCALe:PDIVision?"
Pdiv = GPIB.Read
GPIB.Write "DISPlay:WINDow1:TRACe1:Y:SCALe:RLEVel?"
Rlev = GPIB.Read
GPIB.Write "DISPlay:WINDow1:TRACe1:Y:SCALe:RPOSition?"
Ppos = GPIB.Read


'Turn ON, and average five sweeps

GPIB.Write "SENSe1:AVERage:STATe ON"
GPIB.Write "SENSe1:AVERage:Count 5"


'Turn ON, and set 20% smoothing aperture

GPIB.Write "CALCulate1:SMOothing:STATe ON"
GPIB.Write "CALCulate1:SMOothing:APERture 20"