When running an external program on the PNA, such as a support program, the program may have a dialog that becomes blocked by the PNA application. When this happens, there are several ways to cause your program to again have focus on top of the PNA. An easy way to do this is to cause the PNA App to move to the back of the applications.
This operation must be performed each time the PNA application is selected, which again moves it to the top of another application.
How to Move the PNA App to the Back |
|
|
Using front-panel |
Using Menus |
|
Keyboard shortcut: Alt-f-b |
|
This setting is not programmable |
|