Activating and Deactivating Advanced Mode

Other topics about Advanced Mode

Activating Advanced Mode

  1. Select the Setup tab.

  2. Click Advanced Mode in the More Functions tab, then the Advanced Mode dialog is displayed.

  3. When you want to perform a calibration such as TRL calibration in Advanced Mode, select the check box named Use Advanced Calibration Methods in dialog .

  4. Click Yes to start the Advanced Mode.

  5. The following settings are changed.

Deactivating Advanced Mode (Returning to Basic Mode)

  1. Select the Setup tab.

  2. Click Basic Mode button in the More Functions tab, then Advanced Mode dialog is displayed.

  3. Click Yes to start the Basic Mode.

  4. The application is re-started and all settings are reset.