Create a Modulation Distortion Channel

In this topic:

Modulation Distortion Channel

  1. On the VNA front panel, press Meas > S-Param > Meas Class....

  2. Select Modulation Distortion, then either:

  3. In the Confirm Measurement Class Change dialog, click OK to proceed or Cancel to exit.

  4. The Modulation Distortion Setup dialog will be displayed.

  5. The default Distortion Measurement Parameter is PIn1. This means that the displayed trace is the input power incident on the DUT. This setting is set using the DUT Input selection in the RF Path tab.

Modulation Distortion Converter Channel

  1. On the VNA front panel, press Meas > S-Param > Meas Class....

  2. Select Modulation Distortion Converters, then either:

  1. In the Confirm Measurement Class Change dialog, click OK to proceed or Cancel to exit.

  2. The Modulation Distortion Mixer Setup dialog is displayed.

  3. The default Distortion Measurement Parameter is PIn1. This means that the displayed trace is the input power incident on the DUT. This setting is set using the DUT Input selection in the RF Path tab.