Receiver IF Calibration is an additional process for S-parameter calibration in a Modulation Distortion channel to improve the error term of the IF chain of the VNA. Receiver IF Cal measures the S21 of the thru device at different IF frequencies to compute the correction coefficient. The S-parameter Cal Set contains all of these error terms. The point count used for the receiver IF cal is determined by the tone spacing of the modulated signal and the user’s measurement span.
The receiver IF calibration uses the internal PNA CW source to make the measurement.
Perform the Receiver IF Cal if it is inaccurate or missing. This will be indicated in the Receiver IF Cal dialog as a warning message. An inaccurate Receiver IF Cal occurs when the Start, Stop, Center, or Span setting frequencies do not match the active S-parameter Cal Set.
Note: The following procedure assumes the Receiver IF Cal has never been performed and is therefore not part of the active Cal Set.
Ensure that the Modulation Distortion measurement class to be calibrated is currently active.
Press Cal > Cal Sets & Cal Kits > Cal Set... then select a Cal Set to apply to the active channel.
Press Cal > Main > Other Cals.
Select Receiver IF 
	 Cal.... The following dialog is displayed:
	
	
	The Close button aborts the 
	 calibration.
	If Do not show this dialog again 
	 is checked, the Receiver IF Cal dialog will not be displayed when 
	 a calibration is required.
Click on the Calibrate 
	 IF button. The following dialog is displayed:
	
	
Connect a thru device between the input port and the output port (use a low loss, passive component).
Click on the OK button.
If the calibration was successful, the status message will indicate a valid IF calibration.