Starting and Exiting Phase Noise

In this topic:

Starting Phase Noise Application

How to start Phase Noise

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. On the VNA, press Meas > S-Param > Meas Class....

  2. Select Phase Noise, then click OK.

  3. In the Confirm Measurement Class Change dialog, click OK to proceed or Cancel to exit.

  4. The Phase Noise application is displayed (shown below).

  1. Click Instrument.

  2. Select Meas Class....

  3. Select Phase Noise, then click OK.

  4. In the Confirm Measurement Class Change dialog, click OK to proceed or Cancel to exit.

  5. The Phase Noise application is displayed (shown below).

 

Exiting Phase Noise Application

  1. Select a different Measurement Class for the currently active channel.