Connecting with PathWave Vector Signal Analysis (89600 VSA)

Connecting to the 89600 VSA software allows for greater signal evaluation and troubleshooting.

 

Supported Models

Requirements  

Limitations

Connecting with the 89600 VSA Software

Before connection, make sure that the VSA Software and its license are installed.


VNA Application

  1. Launch Network Analyzer application from Windows Start or Shortcut on the desk top.

  2. Click System >  System Setup > Remote Interface....

  3. Check the HiSlip.

IO Connection Expert

  1. Execute IO Connection Expert from Windows Start.

  2. Click +Add, then select LAN instrument.

  3. Add LAN device dialog box is displayed.

  4. Select Enter Address Tab.

  5. Type your host name in Hostname or IP Address in Set LAN Address

  6. Select HiSlip in Set Protocol

  7. Type your remote name in Remote Name: (TCPIP0::::hislip

    )

  8. Check Allow *IDN Query.

  9. Click Test This VISA address, then confirm if your address is verified correctly.

  10. Click OK.

VSA Application

  1. Execute 89600 VSA application from Windows Start.

  2. Select Utilities > Hardware > Discovered Instruments...

  3. Open SIM option and make sure that the Vector Network Analyzer entry matching your hardware is displayed in the list. If not, check the VSA version.

  4. Click Rediscover icon to find TCPIP0 connection, then the VNA connection will be displayed,.

  5. Select Configurations  tab.

  6. Click +, then select "Keysight Network Analyzer" and click ">" to register your VNA.

  7. Select your VNA  in “Current Analyzer Configuration” option. Then, VSA will connect with VNA to start measurements byVNA.