In this topic:
Using Hardkey/SoftTab/Softkey
Using a mouse
Press Sweep > Source Control > LF Extension.
Ensure that ON is selected in the LF Extension softkey.
Click Stimulus
Select Sweep
Select Source Control
Select LF Extension [on/OFF]
If the frequency is set below 10 MHz and LFE is disabled (OFF), the following dialog is displayed. Pressing OK enables LFE.