Write-only
About Source Power Cal

AbortPowerAcquisition Method


Description

Aborts a source power cal acquisition sweep that is currently in progress.

 VB Syntax

powerCalibrator.AbortPowerAcquisition

Variable

(Type) - Description

powerCalibrator

(object) - A SourcePowerCalibrator object

Return Type

None

Default

Not Applicable

Examples

powerCalibrator.AbortPowerAcquisition

C++ Syntax

HRESULT AbortPowerAcquisition();

Interface

ISourcePowerCalibrator