Write-only
About External Devices

Add (External Device) Method


Description

Adds an external device to the system. This is the same as clicking the New button and editing the name on the Configure an External Device dialog.

Upon creation, all settings on the new device are set to the defaults. The device is not active until set using Ext.Dev.Active.

VB Syntax

extDevices.Add name

Variable

(Type) - Description

extDevices

An ExternalDevices (collection)

name

(String) - Name of the new external device.

Return Type

Not Applicable

Default

Not Applicable

Examples

extDevices.Add 'MySource' 'Creates a new external device

C++ Syntax

HRESULT Add (BSTR name)

Interface

IExternalDevices