Write/Read
About Analyzer Events

AllowEventSeverity Method


Description

Sets event filtering to monitor levels of severity.

 VB Syntax

app.AllowEventSeverity severity,state

Variable

(Type) - Description

app

An  Application (object)

severity

(enum naEventSeverity) Choose from:naEventSeverityERROR
naEventSeverityINFORMATIONAL
naEventSeveritySUCCESS
naEventSeverityWARNING

state

 

(boolean)
True
- monitor
False
- do not monitor

Return Type

Not Applicable

Default

Not Applicable

Examples

app.AllowEventSeverity

C++ Syntax

HRESULT AllowEventSeverity( tagNAEventSeverity severity, VARIANT_BOOL bAllow)

Interface

IApplication