Write-only
About Source Power Cal

ApplyPowerCorrectionValues Method  Superseded


Description

This command is replaced with ApplyPowerCorrectionValuesEx Method.

Applies the array of power correction values to the channel memory and turns correction ON. Perform after completing a source power cal acquisition sweep.

This command does NOT save the correction values. To save correction values, save an instrument / calibration state (*.cst file) after performing a source power cal.

 VB Syntax

powerCalibrator.ApplyPowerCorrectionValues

Variable

(Type) - Description

powerCalibrator

(object) - A SourcePowerCalibrator object

Return Type

None

Default

Not Applicable

Examples

powerCalibrator.ApplyPowerCorrectionValues

C++ Syntax

HRESULT ApplyPowerCorrectionValues();

Interface

ISourcePowerCalibrator