| Description | Calculates the Input or Output frequencies of the mixer setup, applies the mixer setup to the mixer object, and turns the channel ON. Note: There is also a Calculate Method on the Converter Object | ||||||||||||||||||||||||
| VB Syntax | obj.Calculate (port) | ||||||||||||||||||||||||
| Variable | (Type) - Description | ||||||||||||||||||||||||
| obj | A Mixer Interface pointer to the Measurement (object) | ||||||||||||||||||||||||
| port | (enum as MixerCalculation) Port of the mixer for which to calculate start and stop frequencies. Choose from: 
 
 | ||||||||||||||||||||||||
| Return Type | Not Applicable | ||||||||||||||||||||||||
| Default | Not Applicable | ||||||||||||||||||||||||
| Examples | obj.Calculate (mixCalculateOUTPUT) | ||||||||||||||||||||||||
| C++ Syntax | HRESULT Calculate() | ||||||||||||||||||||||||
| Interface | IMixer |