Write-only
About Measurement Parameters

CreateS-Parameter Method


Description

This method creates a new S-Parameter measurement in an existing or new window.

 VB Syntax

app.CreateSParameter chan,recvr,source,[window]

Variable

(Type) - Description

app

Application (object)

chan

(long integer) - Channel number of the new measurement

recvr

(long integer) - Number of receivers

source 

(long integer) - Number of sources

window

(long integer) - Optional argument. Window number of the new measurement. Choose 1 to 4. If unspecified, the S-Parameter will be created in the Active Window.

Return Type

Not Applicable

Default

Not Applicable

Examples

app.CreateSParameter 1,2,1,1 'Creates a new S21 measurement in channel 1 and New window(1)
app.CreateSParameter 1,2,1 'Creates a new S21 measurement in channel 1 and in the active window

C++ Syntax

HRESULT CreateSParameter(long ChannelNum, long RcvPort, long SrcPort, long windowNumber)

Interface

IApplication