Write-only
About Receiver Cal

DataToDivisor Method   Superseded


Description

Note: This property is replaced by DoReceiverPowerCal Method.

Stores the measurement’s data to the measurement’s “divisor” buffer for use by the Normalization data processing algorithm. Normalization is currently supported only on measurements of unratioed power, for purpose of receiver power calibration. If DataToDivisor is called on a ratioed measurement (such as an S-parameter), it will return an error.

 VB Syntax

meas.DataToDivisor

Variable

(Type) - Description

meas

(object) - A Measurement object

Return Type

Not Applicable

Default

Not Applicable

Examples

meas.DataToDivisor

C++ Syntax

HRESULT DataToDivisor();

Interface

IMeasurement