Write-only
About Math Operations

DataToMemory Method


Description

Stores the active measurement data into memory creating a memory trace. The memory can then be displayed or used in calculations with the measurement data.

 VB Syntax

meas.DataToMemory

Variable

(Type) - Description

meas

A Measurement (object)

Return Type

Not Applicable

Default

Not Applicable

Examples

meas.DataToMemory

C++ Syntax

HRESULT DataToMemory()

Interface

IMeasurement