Write-only
 About Path Configurator

DeleteConfiguration Method


Description

Deletes the specified configuration name from the VNA. The factory configurations cannot be deleted. This is the only method of programmatically distinguishing a factory configuration from a user-named configuration.

 VB Syntax

pathMgr.DeleteConfiguration name

Variable

(Type) - Description

pathMgr

PathConfigurationManager (object)

name

(String) Configuration name to be deleted.

Return Type

Not Applicable

Default

Not Applicable

Examples

path.DeleteConfiguration "myMixer"

C++ Syntax

HRESULT StoreConfiguration (long channelNum, BSTR configName );

Interface

IPathConfigurationManager