Write-only |
About Macros |
Description |
Removes a macro from the list of macros in the analyzer. Does not remove the file. Note: There are always 25 macro positions. They do not have to be sequential. For example, you can have number 7 but not numbers 1 to 6. |
VB Syntax |
app.DeleteShortCut item |
Variable |
(Type) - Description |
app |
An Application (object) |
item |
(long integer) number of the macro to be deleted. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.DeleteShortCut 2 |
C++ Syntax |
HRESULT DeleteShortcut(long Number ) |
Interface |
IApplication |