Write-only
About Calibration

DoResponseCal Method


Description

Performs and immediately applies a Response cal. Same as selecting Normalize from the Unguided Cal - Measure Standards page. Learn more.

VB Syntax

cal.DoResponseCal (measParam),(SourcePort)

Variable

(Type) - Description

cal

A Calibrator (object)

measParam

(String) Measurement parameter to correct. It is NOT necessary for this measurement to be present.

SourcePort

(long integer) Source port number to calibrate. Optional for S-parameter measurements. Choose from:

0 - N5264B Measurement Receiver (no source ports).

1 - Calibrate port 1

2 - Calibrate port 2 (default, if unspecified)

3 - Calibrate port 3

And so forth for all available VNA / test set ports.

Return Type

None

Default

Not Applicable

Examples

cal.DoResponseCal "A/R",1

C++ Syntax

HRESULT DoResponseCal(BSTR param, long SourcePort);

Interface

ICalibrator9