Write-only
About ECAL Confidence Check

DoneCalConfidenceCheckECAL Method


Description

Concludes the Confidence Check and sets the ECal module back into the idle state.

 VB Syntax

cal.DoneCalConfidenceCheckECAL

Variable

(Type) - Description

cal

A Calibrator (object)

Return Type

None

Default

None

Examples

cal.DoneCalConfidenceCheckECAL

C++ Syntax

HRESULT DoneCalConfidenceCheckECAL( );

Interface

ICalibrator