Write-only |
About Cal Sets |
Description |
Generate a new ENR file by embedding an adapter to an existing ENR file. |
VB Syntax |
calMgr.ENREmbedAdapter (inENR, s2p, outEnr) |
Variable |
(Type) - Description |
calMgr |
(object) - A CalManager object |
inENR |
(String) Path and filename of an existing ENR file |
s2p |
(String) Path and filename of an s2p file of adapter. |
outENR |
(String) Path and filename of an ENR file to output |
Return Type |
ICal Set Interface |
Default |
Not Applicable |
Example |
calMgr.ENREmbedApater (D:\Original.enr","D:\adapter.s2p","D:\new.enr") |
C++ Syntax |
HRESULT ENREmbedAdapter (BSTR inEnr, BSTR s2p, BSTR outEnr); |
Interface |
ICalManager11 |