Write-only |
|
Description |
Generates the error terms for the specified calibration type, stores the error terms in a Cal Set, saves the Cal Set, and returns the Cal Set GUID. If ALL the data for the cal type has NOT been acquired an error message is returned. Note: The manner in which the calibration is assigned to a Cal Set (Cal Register or User Cal Set) is determined by the setting of RemoteCalStoragePreference. |
VB Syntax |
value = obj.GenerateErrorTerms |
Variable |
(Type) - Description |
value |
(String) - Variable to store the returned GUID or error message. |
obj |
Any of the following: GuidedCalibration (object) SMCType (object) VMCType (object) |
Return Type |
String |
Default |
Not Applicable |
Examples |
string = SMC.GenerateErrorTerms |
C++ Syntax |
HRESULT GenerateErrorTerms(BSTR* calsetGUID); |
Interface |
IGuidedCalibration SMCType VMCType |