Write-only
 

GenerateGlobalDeltaMatchSequence Method


Description

Initiates a global delta match calibration.

Learn more about Delta match calibration.

See example of a complete Delta Match calibration.

 VB Syntax

numSteps = guided.GenerateGlobalDeltaMatchSequence conn,cKit

Variable

(Type) - Description

numSteps

Long Integer - Variable to store the returned number of connection steps required by the Global Delta Match Cal.

guided

GuidedCalibration (object)

conn

String  Connector Type for port 1.

cKit

String  Cal Kit for all ports.

Return Type

Not Applicable

Default

Not Applicable

Examples

guided.GenerateGlobalDeltaMatchSequence “APC 3.5 female”,"85052B"

C++ Syntax

HRESULT GenerateGlobalDeltaMatchSequence(BSTR port_1_conn, BSTR cal_kit, long *num_steps);

Interface

IGuidedCalibration2