Read-only
About Equation Editor

GetLibraryFunctions Method


Description

Returns the functions in an imported (loaded) DLL.

 VB Syntax

functions = equation.GetLibraryFunctions location

Variable

(Type) - Description

functions

(variant) - Array to store the returned functions.

equation

A MeasurementEquation object

location

(string) – Full path and filename of the *.dll to be read.

Return Type

Variant array

Default

Not Applicable

Examples

functions=equation.GetLibraryFunctions “C:\Program Files(x86)\Keysight\Network Analyzer\UserFunctions\Expansion.dll”

C++ Syntax

HRESULT GetLibraryFunctions( BSTR filename, BSTR* functionList);

Interface

IMeasurementEquation