Read-only |
Data Access Map |
Description |
Retrieves frequency tone data from the modulation distortion measurement. |
VB Syntax |
data = meas.GetXDataBuffer DataBufferName |
Variable |
(Type) - Description |
data |
(variant) - Array to store the data. |
meas |
(object) - A Measurement object |
DataBufferName |
(string) – Name of the buffer to be read. Note: The following names assume a 2-port VNA. Also, by default, the parameter names assume that VNA Port 1 is connected to the DUT input and VNA Port 2 is connected to the DUT output. If the RF Path settings are changed from the default, the names will change accordingly. For example, if the VNA has 4 ports and Port 4 is connected to the DUT output, the names will change to "PIn1", "POut4", "S11", "S41", etc.
Choose from: "POut2" - Power Out "PIn1" - Power In "MSig2" - Modulation Signal Out "MDist2" - Modulation Distortion Out "MGain21" - Modulation Gain "MComp21" - Modulation Compression "PGain21" - Power Gain "S11" - Linear Input Match "S21" - Linear Gain "LPin1" - Linear Power In "LPOut1" - Linear Reflected Power In "LPOut2" - Linear Power Out |
Return Type |
Variant array |
Default |
Not Applicable |
Examples |
meas.GetXDataBuffer "S21" |
C++ Syntax |
HRESULT GetXDataBuffer(BSTR DataBufferName, VARIANT* Data ); |
Interface |
IMeasurement19 |