Read-only
About Cal Sets

GetCalSetCatalog Method - Superseded


Description

This method is replaced with EnumerateCalSets

Returns a string containing a list of comma-separated GUIDs in the following format:

{FD6F863E-9719-11d5-8D6C-00108334AE96},

{1B03B2CE-971A-11d5-8D6C-00108334AE96},

{2B893E7A-971A-11d5-8D6C-00108334AE96}

 VB Syntax

value = calMgr.GetCalSetCatalog

Variable

(Type) - Description

value

(string) - Variable to store the returned GUID list

calMgr

(object) - A CalManager object

Return Type

String

Default

Not Applicable

Example

value = calMgr.GetCalSetCatalog

C++ Syntax

HRESULT GetCalSetCatalog( BSTR);

Interface

ICalManager