Read-only |
About Cal Sets |
Description |
Note: This command is replaced by CalSet.getErrorTermList2 Returns the list of Error Terms contained in this Cal Set for the CalType specified in the OpenCal Set method. Learn more about reading and writing Cal Data using COM. The list is a comma separated, textual representation of the error terms with the term name followed by the port path in parentheses: Term (n, n), Term (m,n) Before calling this method you must open the Cal Set with OpenCal Set.. If the Cal set is not open, this method returns E_NA_Cal Set_ACCESS_DENIED. Use StringToNAErrorTerm2 to convert the list entrees to values that can be used with GetErrorTerm and PutErrorTerm. Note: The
port path designation (m n) indicates the ports that contribute to the error
being compensated. Directivity, source match and reflection
tracking are single port characteristics, designated in this list
by (n n) where
n equals the port being characterized. |
VB Syntax |
CalSet.GetErrorTermList (SetID, count, strList) |
Variable |
(Type) - Description |
CalSet |
(object) - A Cal Set object |
SetID |
(long) - specifies the error term set to query. Use 0 for the primary set. |
count |
(long) - the number of error terms in the returned list |
strList |
(string) - comma separated list of error terms found in Cal Set |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
dim count as Integer Assuming the cal set contained the full set of error terms for this two-port Cal, the returned list would be: "Directivity(1 1),SourceMatch(1 1),ReflectionTracking(1 1),TransmissionTracking(2 1),LoadMatch(2 1),Isolation(2 1),Directivity(2 2),SourceMatch(2 2),ReflectionTracking(2 2),TransmissionTracking(1 2),LoadMatch(1 2),Isolation(1 2)" |
C++ Syntax |
HRESULT GetErrorTermList (long etermSetID, long* count, BSTR* strList); |
Interface |
ICalSet |