Read-only
About the External TestSet connector

Get ExternalTestSetIO Method


Description

This method returns the IExternalTestSetIO interface.

 VB Syntax

app.GetExternalTestSetIO

Variable

(Type) - Description

app

An Application (object)

Return Type

IHWExternalTestSetIO

Default

Not Applicable

Example

Dim app As AgilentPNA835x.Application
Dim ets As HWExternalTestSetIO
Set ets = app.GetExternalTestSetIO

C++ Syntax

HRESULT GetExternalTestSetIO (IHWExternalTestSetIO **ptestset);

Interface

IApplication