Read-only |
Description |
Note: this command is replaced by Get SnpDataWithSpecifiedPorts Method. Reads SnP data from the selected measurement. Learn more about SnP that is returned from the VNA. |
VB Syntax |
data = meas.GetSnPData type |
Variable |
(Type) - Description |
|
data |
Variant array to store the data. |
|
meas |
A Measurement (object) |
|
type |
(string) - Type of SnP data to return. If unspecified, <n> is set to 2. Choose from: "S1P" returns 1-Port data for the active measurement if the active measurement is a reflection parameter such as S11 or S22. The behavior is UNDEFINED if the active measurement is a transmission parameter such as an S21. "S2P" returns data for the current 2-port measurement (4 S-parameters). "S3P" returns data for the current 3 port measurement (9 S-parameters). Valid only on instruments with 3 ports or more. "S4P" returns data for the current 4 port measurement (16 S-parameters). Valid only on instruments with 4 ports or more.
SnP data can be output using several data formatting options. See SnPFormat Property |
Return Type |
Variant - 3 dimensional array.
For example: Data(0,5,1) returns the imaginary value of the fifth data point of S11 (if the s2p request includes port #1) |
Default |
Not Applicable |
Examples |
snp = meas.GetSnPData("s1p") |
C++ Syntax |
HRESULT GetSnPData( BSTR snptype, VARIANT * response) |
Interface |
IMeasurement3 |