Description |
Get the calibration standard numbers for a specified calibration class. To set the calibration number use SetStandardsForClass Method |
||||||||||||||||||
VB Syntax |
calkit.GetStandardsForClass (calclassorder, std1, std2, std3, std4, std5, std6, std7) |
||||||||||||||||||
Variable |
(Type) - Description |
||||||||||||||||||
calKit |
A CalKit (object) |
||||||||||||||||||
calclassorder |
(enum NACalClassOrder) Choose from:
|
||||||||||||||||||
std1…std7 |
(long) Calibration Standard Number. Nominal values from 1 through 30. 0 indicates that a standard number has not been selected. |
Return Type |
Not applicable |
Default |
Not applicable |
Examples |
calkit.GetStandardsForClass naRefl_3_S11, std1, std2, std3, std4, std5, std6, std7 |
C++ Syntax |
HRESULT GetStandardsForClass(NACalClassOrder calclassorder, long std1, long std2, long std3, long std4, long std5, long std6, long std7) |
Interface |
ICalKit |