Read-only |
|
Description |
Returns the description of the specified step in the calibration process. For an ECal User Characterization this returns the description of the specified step in the ECal User Characterization process. |
VB Syntax |
value = obj.GetStepDescription (n) |
Variable |
(Type) - Description |
value |
(string) - Variable to store the returned number of steps. |
obj |
Any of the following: GuidedCalibration (object) SMCType (object) VMCType (object) ECalUserCharacterizer (object) |
n |
(Long) Step in the process. Use GenerateSteps to determine the total number of steps. |
Return Type |
String |
Default |
Not Applicable |
Examples |
value = SMC.GetStepDescription(5) |
C++ Syntax |
HRESULT get_GetStepDescription(long step, BSTR* str); |
Interface |
IGuidedCalibration SMCType VMCType IECalUserCharacterizer |