Read-only |
About Segment Sweep |
Description |
Returns the channel's X-axis values. GetXAxisValues is a convenient method for determining the frequency of each point when the points are not linearly spaced - as in segment sweep. See the Measurement2 Interface to learn how this method differs from meas.GetXAxisValues. Note: This method returns a variant which is less efficient than GetXAxisValues2. Note: In Segment Sweep, chan.NumberofPoints will return the total number of data points for the combined segments. |
VB Syntax |
data = chan.GetXAxisValues |
Variable |
(Type) - Description |
|
data |
Variant array to store the data. |
|
chan |
A Channel (object) |
Return Type |
Variant |
Default |
Not Applicable |
Examples |
Dim varData As Variant |
C++ Syntax |
HRESULT GetXAxisValues (VARIANT* xData) |
Interface |
IChannel |