Write only

Initialize Method


Description

Begins a calibration.

Note: chan must be the active channel.

For ECal User Characterization, use Initialize (ECal).

 VB Syntax

obj.Initialize (chan, useCalStorPref)

Variable

(Type) - Description

obj

Any of the following:

GuidedCalibration (object)

SMCType (object)

VMCType (object)

chan

(Long) Channel number to calibrate.

useCalStorPref

(boolean)

True or 1 - Assignment of Cal Set will be based on the setting of the RemoteCalStoragePreference COM property.

False or 0 – If the channel currently has a selected Cal Set, the calibration will be stored to that Cal Set.  Otherwise, the assignment of Cal Set is based upon the setting of the RemoteCalStoragePreference COM property.

Return Type

Not Applicable

Default

Not Applicable

Examples

smc.Initialize(2,True)

C++ Syntax

HRESULT put_Initialize(long channelnumber, VARIANT_BOOL bCalPref);

Interface

IGuidedCalibration

SMCType

VMCType