Write-only |
About Markers |
Description |
Turns All Marker Interpolation ON and OFF for the measurement. Marker interpolation enables X-axis resolution between the discrete data values. The analyzer will calculate the x and y-axis data values between discrete data points. To override this property for individual markers, use the Interpolated property. |
VB Syntax |
meas.Interpolate = value |
Variable |
(Type) - Description |
meas |
A Measurement (object) |
value |
(boolean) |
Return Type |
Boolean |
Default |
True (ON) |
Examples |
meas.Interpolate = 1 |
C++ Syntax |
HRESULT InterpolateMarkers(VARIANT_BOOL bNewVal) |
Interface |
IMeasurement |