Read-Write
About the Cal Wizard

LaunchCalWizard Method


Description

Launches the S-parameter Cal Wizard on the VNA and does not return until the Cal Wizard is dismissed.

To launch the Cal Wizard for a VNA Application, use the LaunchDialog Method.

Note: The Cal Wizard operates on the active measurement. Therefore, activate the measurement to be calibrated before launching the Cal Wizard.

 VB Syntax

success = app.LaunchCalWizard (newCS)

Variable

(Type) - Description

success

(boolean) - variable to store the returned value

True - The Cal was completed

False - The Cal was canceled without completing the calibration.

app

An Application (object)

newCS

(boolean)

True - Cal will be performed on a new Cal Set.

False - Cal will be performed using the existing Cal Set assigned to the channel. If no Cal Set is found, a new Cal Set will be created.

Return Type

Boolean

Default

Not Applicable

Example

dim bSuccess as boolean
dim bNewCalset as boolean
bNewCalSet = false
bSuccess = app.LaunchCalWizard( bNewCalSet)

C++ Syntax

HRESULT LaunchCalWizard(VARIANT_BOOL bCalsuccess)

Interface

IApplication