Write-only |
About Cal Sets |
Description |
Read S parameter of ECal Thru from the ECal memory and save it as s2p file. |
VB Syntax |
ecalMdls.OutputSNPFromECal (kit, ecalstate, snpfile) |
Variable |
(Type) - Description |
ecalMdls |
(object) - A ECalModules correction |
kit |
(String) ECal Model, User char name + " ECal", and serial number of the ECal module used for the characterization, separated by spaces. See examples below. |
ecalstate |
(String) ECal transmission path. Choose from AB, AC, AD, BA, BC, BD, CA, CB, CD, DA, DB or DC. |
snpfile |
(String) Path and filename of the output s2p file name. |
Return Type |
IECalModules Set Interface |
Default |
Not Applicable |
Example |
ecalMdls.OutputSNPFromECal ("N4433A ECal 00001", "BC", "D:\ecalthru.s2p") |
C++ Syntax |
HRESULT OutputSNPFromECal (BSTRkit, BSTR ecalstate, BSTR snpfile); |
Interface |
IECalModules2 |