Write-Read |
SCPI Command Tree |
Description |
Allows the use of COM to send a SCPI command. See a C++ example of how to return error information when using this command. Note: The SCPIStringParser Methods can NOT be used with SCPI Status Reporting. However, the *OPC? will work. |
VB Syntax |
scpi.Parse ("SCPI command") |
Variable |
(Type) - Description |
scpi |
A ScpiStringParser (object) |
SCPI command |
(string) - Any valid SCPI command |
Return Type |
String |
Default |
Not Applicable |
Examples |
Dim scpi As ScpiStringParser |
|
Dim str As String |
C++ Syntax |
HRESULT Parse(BSTR SCPI_Command, BSTR *pQueryResponse) |
Interface |
IScpiStringParser |