Write-only
About Macros

PutShortcut Method


Description

Defines a Macro (shortcut) file in the analyzer. This command links a file name and path to the Macro file. The file must be put in the VNA at the location indicated by this command.

 VB Syntax

app.PutShortcut index,title,path, arguments

Variable

(Type) - Description

app

An Application (object)

index

(long) - Number of the macro to be stored in the analyzer. Use a number between 1 and 25.

If the index number already exists, the existing macro is replaced with the new macro.

title

(string) - The name to be assigned to the macro

path

(string) - Full path, file name, and extension of the existing macro "executable" file.

arguments

(string) - Arguments that may be required for the specified macro to run.

Return Type

Not Applicable

Default

Not Applicable

Examples

app.PutShortcut 1,"Test","C:/Automation/MyTest.vbs",""

C++ Syntax

HRESULT PutShortcut(long Number, BSTR title, BSTR pathname,BSTR arguments)

Interface

IApplication