Write-only |
About Equation Editor |
Description |
Removes an imported an Equation Editor DLL from the VNA. |
VB Syntax |
equation.RemoveLibrary location |
Variable |
(Type) - Description |
equation |
A MeasurementEquation object |
location |
(string) – Full path and filename of the *.dll to be removed. |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
equation.RemoveLibrary “C:\Program Files(x86)\Keysight\Network Analyzer\UserFunctions\Expansion.dll” |
C++ Syntax |
HRESULT RemoveLibrary( BSTR filename); |
Interface |
IMeasurementEquation |