Write-only |
About Cal Sets |
Description |
Saves the current Cal Set to disk. This is the recommended method for saving a Cal Set. Learn more about reading and writing Cal data using COM |
VB Syntax |
CalSet.Save |
Variable |
(Type) - Description |
CalSet |
(object) - A CalSet object |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
myCalSet.Save See Copy Method for an example application of this command. |
C++ Syntax |
HRESULT Save(); |
Interface |
ICalSet |