Write-only |
About Modifying Cal Kits |
Description |
Saves the cal kits, typically after modifying a calibration kit. To load a cal kit into the analyzer from the hard drive, use app.RecallKits. |
VB Syntax |
app.SaveKits |
Variable |
(Type) - Description |
app |
An Application (object) |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
app.SaveKits |
C++ Syntax |
HRESULT SaveKits() |
Interface |
IApplication |