Write-only |
About PNOP Marker Search |
Description |
Initiates a PNOP marker search. Turns on and sets markers 1, 2, 3, and 4 to calculate various PNOP parameters. First set BackOff and PinOffset. To turn off these markers, either turn them off individually or DeleteAllMarkers. To search a UserRange, first activate marker 1 and set the desired UserRange. Then send the SearchPowerNormalOperatingPoint command. The user range applies only to marker 1 searching for the max value. The other markers may fall outside the user range. |
VB Syntax |
pnop.SearchPowerNormalOperatingPoint( ) |
Variable |
(Type) - Description |
pnop |
A PNOP (object) |
Return Type |
Not Applicable |
Default |
Not Applicable |
Examples |
pnop.SearchPowerNormalOperatingPoint |
C++ Syntax |
HRESULT SearchPowerNormalOperatingPoint() |
Interface |
IPNOP |