Write-only
About Balanced Measurements

SetBBPorts Method


Description

For a Balanced - Balanced device type, maps the VNA ports to the DUT ports.

Set the Balanced device type using the DUTTopology Property

 VB Syntax

balTopology.SetBBPorts p1Pos, p1Neg, p2Pos, p2Neg

Variable

(Type) - Description

balTopology

A BalancedTopology (object)

p1Pos, p1Neg, p2Pos, p2Neg

(Long Integer) VNA port number that connects to each of the following DUT ports:

Return Type

Not applicable - To read port mappings, use the BalancedTopology properties.

Default

Not Applicable

Examples

balTop.SetBBPorts 1,2,3,4

C++ Syntax

HRESULT SetBBPorts (long p1Pos, long p1Neg, long p2Pos, long p2Neg)

Interface

IBalancedTopology