Write only
About Power Calibration

SetPowerAcquisitionDevice Method


Description

Sets the power sensor channel (A or B) to be used.  This performs the same function as the Use this sensor only checkbox in the Power Sensor Settings dialog.

Note: This method is only necessary when performing an SMC calibration.

 VB Syntax

pwrCal.SetPowerAcquisitionDevice sensor

Variable

(Type) - Description

pwrCal

(Object) A SourcePowerCalibrator object

sensor

(enum NAPowerAcquisitionDevice) The power sensor channel.  Choose from:

0 – naPowerSensor_A

1 – naPowerSensor_B

Default

Not Applicable

Examples

pwrCal.SetPowerAcquisitionDevice naPowerSensor_A

C++ Syntax

HRESULT SetPowerAcquisitionDevice( tagNAPowerAcquisitionDevice enumAcqDevice);

Interface

ISourcePowerCalibrator3