Write-only
About Balanced Measurements

SetSBPorts Method


Description

For a Single-ended - Balanced device type, maps the VNA ports to the DUT ports.

Set the Single-ended - Balanced device type using the DUTTopology Property

 VB Syntax

balTopology.SetSBPorts se, bPos, bNeg

Variable

(Type) - Description

balTopology

A BalancedTopology (object)

se, bPos, bNeg

 

VNA port number that connects to each of the following DUT ports:

Return Type

Not applicable - To read port mappings, use the BalancedTopology properties.

Default

Not Applicable

Examples

balTop.SetSBPorts 1,2,3

C++ Syntax

HRESULT SetSBPorts (long se, long bPos, long bNeg)

Interface

IBalancedTopology