Write-only
About Marker Functions

SetCenter Method


Description

Changes the center stimulus to the stimulus value of the marker. The start stimulus stays the same and the stop is adjusted.

This command does not work with channels that are in CW or Segment Sweep mode.

 VB Syntax

mark.SetCenter

Variable

(Type) - Description

mark

A Marker (object)

Return Type

Not Applicable

Default

Not Applicable

Examples

mark.SetCenter

C++ Syntax

HRESULT SetCenter()

Interface

IMarker